Loading
IND-360 | Metter Toledo | Studio5000 | Application Code Manager | FTView ME/SE

Ease of integrating a MT IND360 weight indicators via Ethernet/IP

The partnership between Mettler Toledo and Rockwell Automation has allowed the development of libraries such as Add-on, Faceplates (HMI), sample codes, to make integration easy and fast using Application Code Manager.
On this page:
  • Overview
Innovation Center Home Page

What is this for?

The Mettler Toledo IND360 product is a product for accurate weight measurement (load cell) and allows excellent integration with our controllers (ControlLogix, CompactLogix) via Ethernet/IP. The partnership between Mettler Toledo and Rockwell Automation has allowed the development of libraries such as Add-on, Faceplates (HMI), sample codes, to make integration easy and fast. With the Application Code Manager feature (code generator and screens) it is possible to integrate, generate controller application code (Studio 5000), generate HMI screens and network configurations, reducing setup time and startup of production lines and industrial machines.

https://www.mt.com/us/en/home/library/case-studies/industrial-scales/Encompass.html

 

General Features

Our Device Object Libraries allow you to easily interact with Rockwell Automation® Intelligent devices, as drives, motion, network switches, sensors, IoT, and more. The libraries contain tests, documented, and lifecycle. Managed objects that can be used with the manufacturer of machines, processes, and libraries packaged or as stand-alone components. Device Objects Include HMI Faceplates para FactoryTalk® View ME/SE e Studio 5000 View Designer® software and provide a user interface that integrates seamlessly with the goods.

HMI faceplates are standard display files that provide the average user with Interface. These are HMI pop-up screens used to display detailed information related to a specific instruction or device. On systems that follow ISA 101.1 According to design guidelines, front-facing displays are often referred to as Level 4 monitors.

Preconfigured device objects include a supplemental instruction line and a HMI front panel that offers the following benefits:

  • Collect, process, and deliver data between smart devices and Application Logic
  • Detailed collection and delivery of device data
  • Improved device status and diagnostics
  • Common control interfaces that maximize device automation flexibility Selection and reuse of application code

Device objects use cases:

  • Basic device maintenance and diagnostics
  • Virtual device operations for start-up and commissioning
  • Operator and program control for machines and processes Applications

 

Advantages

Integration via Ethernet/IP allows for excellent ease of integration, reducing time and line start-up process. Use of Application Code Manager to generate controller code (Add-on) and general configurations and construction of HMI faceplates for integration.

 

Application Code Manager

Studio 5000® Application Code Manager is a tool that can be used with Device Object libraries to speed up the development of projects and machines. This volume Coding tool allows you to easily design and standardize functionalities with Reusable application code. Enable more efficient project development with reusable code libraries:

  • Quickly create and deploy projects through our app content

 

Libraries

  • Import Rockwell-sourced application content libraries for agility system development.

 

Limitations and drawbacks

Number of IND-360 devices, integrated via Ethernet/IP, depends on the limitation of CIP connections of each controller used.

 

Is this helpful for me?

Integration via Ethernet/IP allows excellent ease of integration, reducing time and start-up of lines, process and industrial machines.

 

How can I make it work?

Hardware

  • PanelView™ 5500 with v8 or later firmware
  • PanelView™ Plus with v10 or later firmware
  • ControlLogix® 5570/5580 controller or CompactLogix™ 5370/5380
  • Controller with v3.01 or later firmware

Software

  • Studio 5000 Logix Designer® v31.02 or later for PAC Application Development
  • Studio 5000® Application Code Manager v4.01 and later for bulk code configuration
  • Studio 5000 View Designer® v8.00 and later for PanelView™ 5000 Application Development
  • FactoryTalk® View Studio v10 and later for PanelView™ Plus or
  • FactoryTalk® View SE Application Development

Required knowledge

  • SO Windows
  • Studio 5000 Design Studio and View Design
  • FactoryTalk View Studio ME
  • FactoryTalk View Studio SE
  • Application Code Manager - Basic

Downloads

Please note: You will need to agree to the Terms & Conditions for each download.

Files for download ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.


Need Help?

If you need help with an application or have feedback from the Innovation Center, please contact us.

Installation Guide

To implement, check the steps below.

Step 1

Manual de Referência: DEVICE-RM905A-EN-P.pdf

 

Localizado em General_Files.zip, no caminho:

MettlerToledoDeviceLibrary_v1.00.00\Reference Manual\DEVICE-RM905A-EN-P.pdf

 

Como importar e configurar objetos de dispositivo Metter Toledo no ACM – Application Code Manager.

Chevron DownChevron Down

Step 2

How to Import and Configure Metter Toledo Device Objects in Studio 5000 Logix Design.

Chevron DownChevron Down

Step 3

How to Import and Configure Metter Toledo Device Objects in FactoryTalk View ME and SE.

Chevron DownChevron Down

Step 4

How to Import and Configure Metter Toledo Device Objects in Studio 5000 View Design.

Chevron DownChevron Down

Step 5

MT-IND360 Visualization & Operational Data - Faceplates.

Chevron DownChevron Down
Have a general inquiry?

Rockwell Automation and our partners offer exceptional industry knowledge to help design, implement, and support your automation investment.

Contact Rockwell Automation
  1. Chevron LeftChevron Left Puerto Rico Chevron RightChevron Right
  2. Chevron LeftChevron Left Sup... Chevron RightChevron Right
  3. Chevron LeftChevron Left Pro... Chevron RightChevron Right
  4. Chevron LeftChevron Left Downloads Chevron RightChevron Right
  5. Chevron LeftChevron Left Innovation Center Chevron RightChevron Right
  6. Chevron LeftChevron Left Ease of integrating a MT IND360 weight indicators via Ethernet/IP Chevron RightChevron Right