Loading
Efficiency | Boiler | Water Heater | FactoryTalk | Studio 5000

Boiler Efficiency

Revision: 0.1 (11/10/2022) - Deploy Time: 60 Minutes | A standard library to calculate Boiler Efficiency in a standardized way with flexibility allows for the same basic building blocks to be utilized.
On This Page:
  • What is this for?
  • Installation guide
Innovation Center Home

What is this for?

The objective of creating a standard Boiler Efficiency library is to gather knowledge from experience and applications utilizing the best approaches to provide features that will be selected based on the detailed requirements of the project scope.  Control, process design, and the configuration approach will utilize a PlantPAx based control system that will be used with standard Boiler Efficiency applications.  It is also desired for the controller to be flexible and allow integration of custom requirements and expansion as future technological developments are realized through industries.

The vision is to allow the user to select specific requirements and procedures, including and configuration capabilities, to meet the needs of the required mixing application. 

Is this useful for me?

Currently, there is no way to calculate Boiler Efficiency in a standardized way. A standard library with flexibility allows for the same basic building blocks to be utilized.

By standardizing the Boiler Efficiency library, it may be used for multiple industries (F&B, Chem, Life Science, Home & Personal Care) across the globe.  This standard will also be able to assist in cost benefit to the organization by lowering the engineer labor to create basic functionality.

Capturing of industry specific knowledge. Future go-to-market features for sales of Plant Pax application. Financial and labor savings are unknown currently.  However, reduced development time is expected due to the ability of tool to create basic functionality.

How can I make it work?

User will enter Boiler system inputs based on standard instrumentation typically used in Boilers.

This first version allows you to have real time efficiency in a Rockwell Automation control system, just import and configure the AOI and the Display, add it in your application and that's it.

System requirements of app:

Item Requirement Version
1 Tool will be built using Steam properties libraries of PlantPAx 4.x – 5.x
2 FactoryTalk View SE/ME 12.00
3 Studio 5000 21 and above
 
 

Process variables will need to be able to be configured including input signal, scaling, and units.

Item Instrumentation
Temperature (Steam and Water) Type:
  • Resistance - RTD with common ranges configurable (PT100, PT1000, etc.) with configurable units: degK, degC, degF
  • mV - Thermocouple with all types for temperature ranges (Type J, Type K, etc.) with configurable and units: degK, degC, degF
  • Analog - analog input signal, with scalable engineering units, with configurable units: degK, degC, degF
  • Digital - networked device, ethernet I/P, profibus, ASi, etc. with configurable units: degK, degC, degFTool will be built using Steam properties libraries of PlantPAx
Flow (Steam, Water, Fuel)

Type:

  • Analog - analog input signal, with scalable engineering units, with configurable units: gpm, gpm, lpm, lph, m3h, kgh, etc.
  • Digital - networked device, ethernet I/P, profibus, ASi, etc. with configurable units: gpm, gpm, lpm, lph, m3h, kgh, etc.
Pressure (Steam, Water) Type:
  • Analog - analog input signal, with scalable engineering units, with configurable units PSI, MPa, etc.
  • Digital - networked device, Ethernet I/P, Profibus, ASi, etc with configurable units: PSI, MPa, etc.
 

Knowledge required

Basic knowledge of programming and configuration in Studio 5000 Logix Designer® software and FactoryTalk® View Site Edition Studio.

Downloads

Please note: You will need to agree to the Terms & Conditions for each download.

General_Files.zip ›
Legal Disclaimer Acceptance. ROCKWELL AUTOMATION WILL PROVIDE ACCESS TO ROCKWELL PRODUCTS (BEST PRACTICES, APPLICATIONS AND KNOWLEDGE) ON THE CONDITION THAT YOU ACCEPT AND COMPLY WITH THE FOLLOWING TERMS AND CONDITIONS. YOU ACCEPT AND AGREE TO BE BOUND BY THE TERMS OF THIS AGREEMENT BY DOWNLOADING, INSTALLING, COPYING, OR OTHERWISE USING PRODUCTS. IF YOU ARE ACCEPTING THESE TERMS ON BEHALF OF ANOTHER PERSON, COMPANY, OR OTHER LEGAL ENTITY, YOU REPRESENT AND WARRANT THAT YOU HAVE FULL AUTHORITY TO BIND THAT PERSON, COMPANY, OR LEGAL ENTITY TO THESE TERMS. IF YOU DO NOT AGREE TO THESE TERMS, DO NOT DOWNLOAD, INSTALL, COPY, ACCESS, OR USE THE PRODUCTS, SOFTWARE AND/OR CLOUD SERVICES. 1. Rockwell Automation retains full ownership and title to all Products and related documentation. No rights or licenses are granted other than those set forth in this Agreement. Company grants to Rockwell Automation a non-exclusive, worldwide, royalty-free, perpetual, non-revocable license to use any feedback Company provides regarding the Products, even if Company has designated the feedback as confidential. Rockwell Automation will be entitled to use the feedback without restriction or compensation to Company. 2. Company may not lease sub-lease, assign, license, sub-license or otherwise transfer any of the Products without the prior written consent of Rockwell Automation. Company may not assign or otherwise transfer access rights to the Products without the prior written consent of Rockwell Automation. Any reverse assembly, reverse engineering, decompilation, and creation of derivative works based on the Products by Company is prohibited. 3. Company acknowledges that Products provided under this Agreement are Rockwell Automation’s Confidential Information and are covered by effective or pending copyrights, patents, trademarks and/or trade secrets of Rockwell Automation, and Company agrees to maintain confidentiality by not disclosing Products or documentation to any third party without the prior written consent of Rockwell Automation and to protect the confidentiality of the Products as it would Company’s own confidential information. Company agrees that its obligation of confidentiality under this paragraph shall survive expiration or termination of this Agreement. 4. Company agrees that Products provided under this Agreement are prototypes and examples and its application and results may vary depending on each customer and project conditions. Rockwell Automation do not warranty the same results. This Agreement shall in no way be construed as a commitment by Rockwell Automation at any time to manufacture and/or offer Products for sale. There is no explicit or implicit service level agreement associated with using the Products. Rockwell Automation does not warrant that the functions contained in the Products will meet Company’s requirements. Company agrees to use all Products only in accordance with the instructions and only for the intended usages identified in the documentation. 5. EXCLUSION OF WARRANTIES AND LIMITATION OF LIABILITY. THE PRODUCTS ARE PROVIDED "AS IS". ROCKWELL AUTOMATION DISCLAIMS ANY AND ALL WARRANTIES, EXPRESS, IMPLIED OR STATUTORY, INCLUDING WITHOUT LIMITATION ANY WARRANTIES OF MERCHANTABILITY OR FITNESS FOR A PARTICULAR PURPOSE. ROCKWELL AUTOMATION EXPLICITLY DISCLAIMS ALL WARRANTIES OF NON- INFRINGEMENT AND EXPRESSLY DOES NOT WARRANT THAT THE PRODUCTS, IN WHOLE OR IN PART, WILL BE ERROR FREE OR FREE FROM SECURITY VULNERABILITIES. IN NO EVENT SHALL ROCKWELL AUTOMATION BE LIABLE FOR (i) LOST PROFITS, LOST SAVINGS, DOWNTIME, SPECIAL, INDIRECT OR CONSEQUENTIAL DAMAGES OF ANY KIND, OR (ii) ANY PERSONAL INJURY, PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE ARISING OUT OF OR IN CONNECTION WITH THIS AGREEMENT, WHETHER IN AN ACTION IN CONTRACT, STRICT LIABILITY OR IN TORT INCLUDING NEGLIGENCE. 6. COMPANY AGREES TO INDEMNIFY AND HOLD ROCKWELL AUTOMATION HARMLESS FROM ALL COSTS, AWARDS, DAMAGES, EXPENSES AND FEES (INCLUDING ATTORNEYS FEES) RESULTING FROM OR RELATED TO ANY THIRD-PARTY CLAIMS (INCLUDING EMPLOYEES AND AGENTS OF COMPANY) AGAINST ROCKWELL AUTOMATION, ITS DISTRIBUTORS, AGENTS, OFFICERS, DIRECTORS OR EMPLOYEES FOR PERSONAL INJURY (INCLUDING DEATH), PROPERTY DAMAGE OR ENVIRONMENTAL DAMAGE RELATED TO OR RESULTING FROM THE USE OF THE PRODUCTS. 7. In the event a Product is exported, Company agrees to comply with all applicable United States Export Control Law and Regulations, and the applicable export control laws of other countries. This Agreement shall be governed by the laws of the state of Wisconsin. This Agreement is the complete and exclusive Agreement between Rockwell Automation and the Company, and supersedes all prior agreements, whether written or oral, relating to the Products.

Need Help?

If you need help with an application or have feedback from the Innovation Center, please contact us.

Installation Guide 

Step 1:

1. Import file L5X for routine according with the programing language to use:

  • Calc_Boiler_Efficiency_FB_Routine_FBD. L5X for Function Block.
  • Calc_Boiler_Efficiency_LD_Routine_RLL.L5X for Ladder.

Note: Please read the instructions in the program comments

  • Step 1 - Image 1

  • Step 1 - Image 2

  • Step 1 - Image 3

Step 1 - Image 2

Step 1 - Image 3

Step 2

Import the Global Object in FTView SE Application.

  • Boiler efficiency.ggfx.
Have a general inquiry?

Rockwell Automation and our partners offer exceptional industry knowledge to help design, implement, and support your automation investment.

Contact Rockwell Automation
  1. Chevron LeftChevron Left Puerto Rico Chevron RightChevron Right
  2. Chevron LeftChevron Left Sup... Chevron RightChevron Right
  3. Chevron LeftChevron Left Pro... Chevron RightChevron Right
  4. Chevron LeftChevron Left Downloads Chevron RightChevron Right
  5. Chevron LeftChevron Left Innovation Center Chevron RightChevron Right
  6. Chevron LeftChevron Left Boiler Efficiency Library Chevron RightChevron Right