Loading
Capability

Customized Lockout/Tagout Training to Meet Your Needs

We Can Develop and Deploy Your Compliant Lockout/tagout Training Program
two people in safety gear review lockout/tagout training
Safety Solutions
  • LOTO Program Services
  • Procedures
  • Auditing
  • Training
  • Policy
  • Device Recommendations
  • ScanESC Software

Training is an essential and required component of your lockout/tagout program (LOTO). In fact, OSHA states in 1910.147(c)(7) that employers are required to provide training to all their authorized and affected employees.  Employers must retrain employees if there is a change in their work assignment, machine, and/or process or if there are any deficiencies in the authorized or affected employees’ understanding and use of lockout/tagout procedures.

Our lockout/tagout training specialists help minimize uncertainties and misconceptions involved with lockout/tagout and will save you valuable time and resources while keeping you compliant.

How Do You Comply with Lockout/Tagout Training?

Training Requirements for Authorized and Affected Employees

OSHA mandates that employees have the necessary knowledge and skills to comply with your company’s lockout/tagout program.  It is the responsibility of the employer to verify that personnel understand the appropriate lockout/tagout components and how they apply within your specific industry.

It is also important to recognize the different types of employees defined in the lockout/tagout standard, and to ensure that each employee receives the appropriate training. An affected employee is someone who operates equipment, or works near equipment that requires lockout/tagout but who does not service or maintain it. An authorized employee is an individual who performs service or maintenance on a piece of equipment, and therefore is responsible to lock and tag it out. Training should discuss these differences and make each type of employee aware of their specific responsibilities.

In addition, OSHA requires that authorized employees must be trained to recognize hazardous energy sources. They need to understand how energy sources might be labeled inside a plant, so that they are prepared to work with them.

Further, authorized employees need to understand what types of energy exist, and the magnitudes of each type available in the workplace, so that they are aware of the risks involved. They should be trained how to isolate each type of energy source, to make sure it is controlled properly.

Affected employees simply need to understand the purpose and use of the lockout/tagout procedures. It is vital that affected employees recognize that they must not interfere with equipment that has been locked out. All other employees who may pass through the area must also have general awareness of lockout/tagout and their responsibilities.

Which employees can perform lockout/tagout?
Which employees can perform lockout/tagout?
Blog
Blog
Which employees can perform lockout/tagout?
To service or perform maintenance on equipment, an authorized employee must follow lockout/tagout procedures outlined by the employer.
Read Now

An Overview of Our Lockout/Tagout Training Program

A Complete Overview of Lockout/Tagout Procedures
Main Image
Brochure
A Complete Overview of Lockout/Tagout Procedures

Everything you’ve ever wanted to know about lockout/tagout procedures, from the history of LOTO procedures and specific OSHA regulations to the benefits of compliance.

Download Now

Implement a Successful Program with Quality Training

For authorized employees, they must have the knowledge and skills necessary to safely apply, use, and remove energy isolating devices. The trainings must include the following information:

  • How to recognize hazardous energy sources.
  • The types of energy at the facility and the magnitudes of the sources.
  • Instruction on how to use the energy-control procedures, including the methods and means to isolate and lock out those energy sources.

Affected employees, though they do not require the same level of training as authorized employees, must receive training in the purpose and use of energy-control procedures. They must be trained to do the following:

  • Recognize when the energy-control procedure is being used.
  • Understand the purpose of the procedure.
  • Understand the importance of not tampering with lockout or tagout devices.
  • Not attempt to restart or use equipment that has been locked out.
Need Lockout/Tagout Assistance?

We offer industry expertise to help design, implement and support your automation investment

Have a LOTO Specialist Contact You

Recommended for You

Safety and Risk Management in the Age of IIoT
Main Image
White Paper
Safety and Risk Management in the Age of IIoT

This eBook sheds new light on the business value of safety. It shows a clear association between the adoption of safety and risk management best practices and operational benefits.

Download Now
Loading
Loading
Maintaining Proper Safety During Times of Change
Upcoming
On-Demand
Maintaining Proper Safety During Times of Change
Webinar
Maintaining proper safety during times of change - are you ready?
Date: September 15, 2020
Time:1:00 P.M. Central Daylight Time
Duration: 60 Minutes
Language: English
View this Session
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Capabilities
  3. Chevron LeftChevron Left Lockout/Tagout Program Services
  4. Chevron LeftChevron Left Lockout/Tagout Training Requirements