Loading
Press Release | November 28, 2022
Recent ActivityRecent Activity

Rockwell Automation Simplifies Smart Machine Development, Improves Micro800 Controllers and Design Software

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Machine builders can save engineering time and costs with the enhanced Allen-Bradley Micro850 and Micro870 2080-Lx0E controllers using the latest Connected Components Workbench software from Rockwell Automation.

The improved 2080-Lx0E controllers offer greater connectivity and design efficiency through the new Class 1 implicit messaging capability with up to eight EtherNet/IP devices support. The 2080-Lx0E controllers streamline integration of controller to drives, supporting PowerFlex 520 series and Kinetix 5100 drives over EtherNet/IP with pre-defined tags and pre-developed user-defined function block (UDFB) instructions. More significant is the easy programming and simpler workflow through a familiar and intuitive design environment.

Connected Components Workbench software version 21 is the required minimum to support the Class 1 implicit messaging capability in Micro850 and Micro870 2080-Lx0E controllers. The controller and software enhancements can help drive industrial operations productivity while lowering costs. Users can benefit from a more connected and simplified control system for their automated designs.

Users can minimize programmatic efforts and troubleshooting time, which simplify the development of standalone machines that are built with the Rockwell Automation Micro Control System. The expanded smart capabilities allow users to develop and deploy automation projects faster, which can accelerate time to market and drive business growth. 



Allen-Bradley, Connected Components Workbench, Kinetix, Micro800, Micro850, Micro870, PowerFlex and Rockwell Automation are trademarks of Rockwell Automation Inc.

PowerFlex 6000T motor controller


Published November 28, 2022


  1. Chevron LeftChevron Left Puerto Rico Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right