Loading
Press Release | April 08, 2021
Recent ActivityRecent Activity

Increase Productivity with New Smart Signaling Solution from Rockwell Automation

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

The new Allen-Bradley 856T Control Tower Stack Light system provides maximum flexibility in meeting the widest range of applications with fewer components. This system uses a modular design that incorporates brighter LED illumination and a broad offering of sound technologies. All signals in the system are 24V AC/DC powered, which means that just three power modules can cover the entire system. The latest additions to the 856T Control Tower Stack Light family are IO-Link enabled versions that provide diagnostic information and ease integration into a Connected Enterprise. 


Click to download image.


With greater requirements for production and machine information comes the need for industrial-grade smart devices. Smart devices are integral components for smart machines and crucial to capturing operational data. These smart devices provide real-time insight into the status of a control system, resulting in smarter, more informed decisions. By choosing IO-Link enabled versions of Bulletin 856T Control Tower Stack Lights, users can monitor tower light and machine status in real-time, while allowing for simple remote set-up and troubleshooting.

Smart devices, such as the 856T IO-Link tower light, are foundational to smarter machines and equipment, smart systems and knowledge-driven operations. They are often the first step in a digital transformation because they deliver raw, real-time data. This valuable information can reduce one of the most significant issues – unplanned downtime. Improve productivity with information that starts at the plant floor with devices that enable predictive maintenance, pinpoint performance issues and reduce repair time.

Allen-Bradley and Control Tower are trademarks of Rockwell Automation Inc. Trademarks not belonging to Rockwell Automation are property of their respective companies.




Published April 8, 2021


  1. Chevron LeftChevron Left Puerto Rico Chevron RightChevron Right
  2. Chevron LeftChevron Left Company Chevron RightChevron Right
  3. Chevron LeftChevron Left News Chevron RightChevron Right
  4. Chevron LeftChevron Left Press Releases Chevron RightChevron Right