Loading
Case Study | Food and Beverage
Recent ActivityRecent Activity

Sleeman Breweries Increases Production Capacity by 50 Percent in Two Weeks with Virtualized Process Automation System

Process automation system from Rockwell Automation provides internal process and recipe control

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Draft Beer

Challenge

  • Increase production capacity to meet growing consumer demand; avoid high expense of building a new greenfield facility.

Solutions

  • PlantPAx Distributed Control System - Enables easy access of information to operators and executive-level.
  • FactoryTalk Brew - This solution provides control of brewing processes, advanced reporting and analytics.
  • VMWare Virtualized Servers - Deliver redundant data storage.

Results

Grew Production

  • Increased production levels by 50 percent within two weeks without adding production equipment.

Improved Process Control

  • Gained control over production, with in-house ability to easily make process and recipe changes.

Capital Costs

  • Avoided need to build new facility or add equipment.

Taking Advantage of the Boom

Ten years ago, tourists looking for a taste of the local life in Southern Canada may have asked for one of the region’s best wines. Today, it’s all about craft beer.

From entrepreneurial newcomers to large-scale producers, brewers in Canada are cashing in on the thirst for craft beer. The number of microbreweries – ­producing less than 25,000 cases of 24 – has more than doubled in the last seven years.

The explosion in craft beer popularity had one company – Sleeman Breweries – bursting at its production seams. The third-largest brewer in Canada, Sleeman brews and distributes popular beers from lagers to pale ales.

With a notorious past in bootlegging and a brewing history dating back to 1834, the company has re-emerged as a powerful presence in the craft beer market. Sleeman operates three brewing production facilities located in Ontario, Quebec and British Columbia.

Modernizing Craft Brewing

An increase in craft beer demand is ideal for a company like Sleeman, but running out of production capacity is not. At its Okanagan Spring Brewery (OSB) in Vernon, British Columbia, the company was struggling to meet market demand for its OSB beers. The management team was looking for ways to increase output beyond the maximum of eight brews per day.

If unable to increase production capacity at OSB, the company could be faced with the need to build a new facility at a high capital investment cost.

At the time, Sleeman had engaged third parties to produce enough to meet customer demand – not ideal for managing costs, ensuring consistent quality and flavor, and meeting delivery deadlines.

Not only was the facility limited in its ability to increase production, the existing infrastructure was based on an antiquated, semi-automated control system. Changes to the brewing process –  including adding new recipes – needed to be made manually, which increased the risk of human error or inconsistencies.

Throughout the production process, operators needed to be at the right place at the right time. If the operator was not on the line to move production forward, brewing would be on hold.

These constraints limited Sleeman’s ability to respond quickly to changes in consumer taste or trends in the industry. The manual approach also hampered access to accurate and timely production metrics needed to fully control the brewing process.

Batch reporting was ad hoc and required operators to input numbers on paper, limiting real-time access to critical information such as pressure and flow rates.

Better Control Means Better Brews

The Sleeman team worked with McRae Integration, a Rockwell Automation Recognized System Integrator, to design and implement an integrated process automation system to increase capacity, reduce risk and provide access to real-time production data.

The Sleeman team was hoping to standardize on one solution across its facilities. A single platform would enable executives to view production metrics and operations data for all facilities from the corporate location.

With one common platform, in-house mechanics and electricians also could more easily transition from one facility to another and keep parts storage streamlined.

“A single platform would give us insights across the line and between facilities, so we could build on successes and meet our goals for continuous improvement while continuing to make great beer,” said Stefan Tobler, brewmaster at OSB. “We had already standardized on Rockwell Automation equipment at our other facilities, and knew McRae could help us meet our goals with a single platform based on the Rockwell Automation technology.”

McRae implemented a phased approach based on the PlantPAx® distributed control system (DCS) from Rockwell Automation and McRae’s own Meridian BrewSoft and BrewSight software, now FactoryTalk® Brew™.

The system includes reporting and historian software that collects, tracks and records key process data to pinpoint brew cycle trends, allowing operators to proactively make changes to brews as needed. The Rockwell Automation library of process objects provides predefined controller code and faceplates, and the new system helps Sleeman operators more quickly configure new batches and build recipes.

McRae customized the solution for brewing applications with its software solutions, which provide operators with complete control of the process through easily operated web interfaces.

Allen-Bradley® PowerFlex® 525 and PowerFlex 755 drives from Rockwell Automation deliver flexible motor control in the brewing process and help communicate device diagnostics to the control system.

To complete the implementation, McRae worked with Sleeman’s IT team to install VMware® virtualized servers. The Sleeman team had implemented redundant servers at its Vernon facility a few years earlier, but found the costs of the equipment and additional storage space difficult to maintain.

The VMware virtualized servers provided automatic redundancy for production data with enhanced data recovery and expanded data storage. One virtualized server can replace up to four physical backup servers, which greatly decreases the equipment hardware costs.

It also provides the Sleeman team with the ability to create copies of the virtualized servers to run simulations offline and test production changes before they are made.   

Ready for More Beer

Within two weeks of the implementation, Sleeman increased production by 50 percent at its Vernon facility going from eight brews to 12 brews per day.

The brewing team can now complete all brews on-site without using third-party producers. And they have avoided the cost of a new facility or significant equipment upgrades or additions.

Additionally, operators have gained more control over the brewing process. With web browser-based recipes, operators can more easily build a new recipe, create a test batch, and store the recipe in the system for additional testing and production.

Brewing managers can simply make process and recipe changes via a web browser interface, without additional personnel.

Management can check on any production issues leveraging the PlantPAx system’s trending capabilities and the BrewSight software’s reporting. With exception reporting, the system creates reports to track progress as the brews reach fermentation and emails management if any brew variables deviate.

The brewing team can take any corrective action needed and reduce downtime, rather than reworking and blending off the brew in small amounts later.


Within two weeks of the implementation, Sleeman increased production by 50 percent at its Vernon facility going from eight brews to 12 brews per day.


“Craft brewing involves a lot of small changes in recipes – based on water, incoming malt and other variables – plus adding new recipes,” said Tobler. “The PlantPAx system with FactoryTalk Brew software allows us to maintain brew quality, while also providing the flexibility we need to quickly respond to changing consumer tastes and market trends.”

The software upgrades have kept the brew quality high while increasing production speed. The Vernon facility now has an industry-leading, two-hour brew cycle, with improved consistency in flavor and quality.

The Sleeman team is not done – they plan to implement the PlantPAx platform throughout the rest of the Vernon facility, including the tank farm and packaging lines. As the standardization across all areas of Sleeman’s facilities expands, corporate visibility will improve, allowing the company to more effectively make decisions that will grow their business.

The results mentioned above are specific to Sleeman Breweries’ use of Rockwell Automation products and services in conjunction with other products. Specific results may vary for other customers.

Allen-Bradley, FactoryTalk Brew, PlantPAx and PowerFlex are trademarks of Rockwell Automation Inc.; VMware is a trademark of VMware Inc.

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies