Loading
Case Study | Industrial Automation
Recent ActivityRecent Activity

VK Logic Utilises Rockwell Automation Technology to Power Unique Mobile Grain Handling Solution

Klean A Seed Yarrawonga enjoys the benefits of automation with an upgraded seed grading machine.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
The new mobile seed grading machine features a unique telescopic arm, allowing the machine to fill multiple silos from the one position.

Challenge

  • Klean A Seed required an increase in grain-handling capacity, which had to be designed within strict weight and size limits of the truck.
  • Full cleaning and decontamination processes are required between customers, and need to be done efficiently in order to minimise downtime.

Solutions

  • CompactLogix™ safety processor
  • PowerFlex 525 drive over Ethernet
  • PanelView™
  • PowerFlex 750 drive

Results

  • Increased capacity – The new grain handling solution comfortably achieves 36 tonnes per hour, well above the level of 32 that was sought from the outset.
  • Faster cleaning – With easy access to cleaning all parts of the truck, cleaning times can be reduced from 30 minutes to 5-6 minutes each time.
  • Greater machine control – Rockwell technology has enabled greater control over the grain handling machine and its components.

A VK Logic solution, powered by Rockwell Automation technology, is helping to enhance uptime and increase capacity for professional mobile seed grading business, Klean A Seed.

Major benefits of the new solution include an increase in capacity to 36 tonnes, quality assurance, better contamination control, and more efficient cleaning.

The technology involved recognises that grain handling is a complex process that requires dedication to quality, hygiene, and uptime. To produce a clean, graded final product suitable for vendors or re-sowing, grains are typically taken offsite to a processing facility.

VK Logic used Rockwell Automation technology to create a unique mobile grain handling solution that is delivering uptime and efficiency benefits to Klean A Seed.

VK Logic used Rockwell Automation technology to create a unique mobile grain handling solution that is delivering uptime and efficiency benefits to Klean A Seed.

Carting seed to and from a processing facility adds delay and expense, so Pat Cummins established a mobile grain processing business, Klean A Seed, in Yarrawonga, about 100km west of Albury/Wodonga, on the Victorian border with NSW. Klean A Seed provides seed grading, grain processing, contamination control, and quality seed treatments.

“I work with farmers to treat winter cereals, like wheat and barley, and prepare them for sowing. Klean A Seed helps with pest and disease control, and our professional seed grading helps avoid blockages of planting machinery,” says Cummins, who has owned and operated Klean A Seed since 2009.

After years of providing a mobile seed grading service, Cummins noticed several areas that could be more efficient, produce higher quality results, and enhance profitability, if the right technology was used.

Taking mobile seed grading to the next level

After thorough research, Cummins engaged VK Logic, a specialist design, build, and automation company based in North Albury, to build a new truck utilising the latest technology.

“There were a number of challenges in developing the Klean A Seed solution. Pat had a great vision for what he wanted to achieve, but there were restrictions in what could fit in the size and dimensions of the truck, while still keeping it roadworthy and safe for on-road and off-road use,” said Justin Van Klaveren, managing director, VK Logic.

VK Logic provides total end-to-end engineering solutions, including in-house engineering and fabrication, with a combination of mechanical, electrical, and automation expertise. Having design, building, and maintenance capabilities under one roof means projects can be completed more efficiently compared to engaging two or three separate companies.

“To keep the truck within certain dimensions and weight distributions, but to add such advanced technologies and processes, was one of the largest challenges of the project. We found Rockwell Automation’s technologies gave us the greatest flexibility to achieve these complex requirements,” added Van Klaveren.

VK Logic identified key areas that could be improved in the new truck build, including making it more user-friendly, giving the operator greater control over machines and processes, increasing capacity, and reducing maintenance downtime.

The new mobile seed grading machine features a unique telescopic arm, allowing the machine to fill multiple silos from the one position.

The new mobile seed grading machine features a unique telescopic arm, allowing the machine to fill multiple silos from the one position.

“We knew, given the complex requirements, that the best process control solutions could be achieved using Rockwell Automation technologies. Not only was Pat already familiar with Rockwell gear, but Rockwell Automation provides greater accessibility to support when out in the field, which is a crucial benefit to a business that spends its time in the countryside helping farmers,” said Van Klaveren.

Rockwell Automation technology gave Klean A Seed greater control over the machine, leading to efficiency and performance benefits.

Rockwell Automation technology gave Klean A Seed greater control over the machine, leading to efficiency and performance benefits.

New technology drives performance benefits

VK Logic designed a new mobile seed grader that utilised Rockwell Automation’s CompactLogix™ safety processor, PowerFlex 525 drive over Ethernet, PanelView™, and PowerFlex 750 drive.

“Rockwell Automation had the best product offering and solutions to complement the new truck we were building, and the service is a valuable added benefit,” said Van Klaveren.

The unique design of the new mobile seed grader featured a range of innovative advances on previous designs, including:

  • A conveyor belt with 3.6m telescopic function, so that Klean A Seed can transfer the treated seed directly into the customer’s silo. Further, the conveyor can then be adjusted, so that it can deposit seed into different silos within reach, without having to adjust the position of the truck
  • Slide-out generator, for easy access and maintenance
  • More electric motors, controlled via Rockwell Automation PLCs (Programmable Logic Controllers), which provides more control over the machine
  • Flatbed type screens and rotary screens for grain processing

“VK Logic, a Rockwell Automation System Integrator Silver partner, has done an outstanding job of listening to customer needs, and developing the most efficient and user-friendly solution, one that will continue to deliver value year after year,” said Matthew Taylor, NSW account manager, Rockwell Automation.

Increased capacity and uptime

With the new truck now in operation, Cummins is experiencing a broad range of benefits in relation to capacity, user-friendliness, and maintenance.

“One of the major objectives of the project was to increase capacity. We nominated 32 tonnes per hour from the outset, and now that the truck is fully built, it is comfortably achieving 36 tonnes per hour, which is a great result,” added Van Klaveren.

Maintenance was another major consideration in the new truck’s design. To avoid contamination, and to provide quality assurance to customers, Klean A Seed needs to clean out the entire machine between customers.

VK Logic designed the truck so that the machinery tilts out, which makes access for cleaning significantly easier, thereby reducing downtime. “We estimate that a 30-minute cleaning task has now been reduced to 5 or 6 minutes each time. When you consider how many customers Pat is serving, that time saving really adds up,” said Van Klaveren.

“We are proud of this solution, and the ongoing benefits it will deliver to Klean A Seed. Rockwell Automation gave us the technology features, the flexibility, and the service to recommend a robust solution to our customer, so it was an ideal partnership,” he concluded.

Published August 18, 2022

Topics: Industrial Automation & Control
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Case Studies