Loading
Blog | Motor Control Centers
Recent ActivityRecent Activity

Top 3 Design Features for a Safer Motor Control Center (MCC)

Is your motor control center designed with safety in mind? Here are our top three design features for a safer motor control center.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Top 3 Design Features for a Safer Motor Control Center (MCC) hero image

If an uncontrolled arc flash occurs within an MCC, the result is downtime, expense and most concerningly, employee injury. With five to 10 arc explosions occurring every day in the United States, the risk is real.

We know that in manufacturing, time equals money, and downtime can have a catastrophic impact on the bottom line. Roughly 82% of companies have experienced downtime in the last three years. Estimates show that each outage can cost a company as much as $260,000 USD per hour.  When combined with the cost to replace the damaged equipment, these failures can be financially devastating.  On top of that, there’s an impact that can’t be calculated in purely financial terms, the risk of injury to your most valuable assets: your employees. Let’s look at the numbers just for the U.S.:

  • An average of 1952 people are injured by electricity each year
  • Between 2012 and 2016 a total of 739 workers died from exposure to electricity. That equates to nearly 3 deaths every week over the 5-year period

So, what can you do to make your MCCs safer? Here are our top three safety design feature picks:

Bus design: How the horizontal power bus is designed and where it’s located in the MCC can both make a big difference in terms of safety. The horizontal bus in a CENTERLINE® MCC is located at the back of the MCC in the vertical center. Automatic shutters immediately isolate the vertical bus when a unit is removed, minimizing potential exposure to an energized bus. Robust, low maintenance design features reduce the likelihood of hotspots or failure. CENTERLINE MCCs have fully supported horizontal bus bars rather than point bracing. For additional bus design safety, CENTERLINE MCCs are available with insulated horizontal bus.  This helps protect the busbar and can prevent an arc from occurring due to tools, animals, dust, or other surprises.

Ability to disconnect power with door closed: The ability to disconnect or connect the power from an individual MCC plug-in unit without opening the enclosure door minimizes personnel exposure to electrical hazards. With SecureConnect™ technology, available for CENTERLINE MCCs, a multi-point validation system verifies that power has been disconnected before ever opening the enclosure door. The system allows you to more safely perform work on or remove a unit without taking the entire system offline. Unlike traditional racking systems, disconnecting a unit with SecureConnect technology is quick and easy. Because this movement is quicker than with a racking system, there is a decreased risk of arc faults occurring when power stabs are being connected or disconnected.

Arc containment solution: Any supplier who claims to have a motor control center with arc containment should:

  • Be able to produce a third-party test certificate that certifies results at a specific voltage, available current and time duration. Be sure to ask for relevant safety certificates before making a purchase.
  • Have testing in multiple locations within the MCC (units, bus compartments, wireways, etc.). Some manufacturers will only test in the vertical bus locations, which is one of the easier locations to pass.
  • Meet the complete IEC/TR 61641 standard for IEC installations, or IEEE C37.20.7 for NEMA installations.

If a manufacturer can’t provide documentation that they meet these criteria, their equipment may not be arc resistant, putting you and your assets at higher risk!

Ready to pick a safer motor control center? Learn more about the CENTERLINE family of MCCs.

Published September 25, 2020

Topics: Motor Control Centers, Low Voltage

Mark Ossanna
Mark Ossanna
Senior Product Marketing Specialist, Rockwell Automation
Product Specialist for 2500 IEC LVMCC. In Industrial Automation for 38 years, 11 Years with Rockwell Automation in LV MCCC/Milwaukee.
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Low Voltage Motor Control Centers
Main Image
Hardware
Low Voltage Motor Control Centers

CENTERLINE® Low Voltage Motor Control Centers (MCCs) offer a rugged, high performance packaging solution for all your motor control needs, providing the advantages you need in your competitive environment.

Get Started
When Did You Think of Your Motor Control Centres?
Main Image
Blog
When Did You Think of Your Motor Control Centres?

Motor Control Centres (MCCs) power just about every manufacturing facility in the world, but do these unsung heroes get the attention they deserve? And what is the cost of MCC failure?

 

Read Now
Acadian Seaplants Grows Capacity by 40 Percent
Main Image
Case Study
Acadian Seaplants Grows Capacity by 40 Percent

Acadian Seaplants used EtherNet/IP MCCs to expand processing capacity with lower hardwiring costs.

Read Now
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs