Loading
Blog | Life Sciences
Recent ActivityRecent Activity

Set Up a Single Use System for Success: Part 1

Early decisions make a lasting impact on a life sciences facility’s growth potential, flexibility and efficiency.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
A life sciences professional wearing coveralls, a mask and safety glasses examines an automated pharmaceutical production line inside a manufacturing facility.

When small and mid-size biological producers decide to incorporate single-use systems in their manufacturing facility, a long list of other critical decisions soon follows. But one of the most impactful choices they make, especially when building a facility, is the process control system.

To ease compliance, reduce batch cycle times and get to market faster, these companies need integrated production processes and information-driven operations — capabilities found in the traditional large, monolithic distributed control systems (DCS). What those systems don’t provide is the flexibility required to meet production needs for smaller-volume processes using single-use equipment.

Equipment-level automation isn’t an ideal option, either. This approach — where each unit operation has a dedicated control system and user interface — creates challenges for the system administrator, such as islands of automation that complicate centralized data collection and user account management.

There’s a better approach to automation that builds for the future. A modern DCS allows producers to incorporate plug-and-play equipment in a scalable, flexible, secure system that uses the latest technology (e.g., industrial ethernet, faster controllers, scalable distributed software) and practices (e.g., cyber-security standards). With a flexible system in place, you’re able to:

  • Evolve operations over time
  • Meet regulatory requirements
  • Reduce validation effort
  • Incorporate newer digital technologies and analytics
  • Lower the total cost of ownership

For those outcomes to occur, you need to lay the foundation early in the process of building a new facility with single-use equipment. By making the correct choices in key areas during the design phase, you’ll feel the impact throughout the life of your facility. We’ll cover two of those areas right now and then the remaining four in Part 2 of this blog.

Network infrastructure

A good starting point for designing a control system is the network infrastructure. Producers should consider how a facility’s communications backbone will meet current needs with simplified connections and seamless data access, while providing the flexibility and scalability needed to accommodate future operational and technology changes.

Legacy fieldbus network protocols used in many pharmaceutical plants today can create challenges in a single-use facility. For example, data limitations can restrict a producer’s ability to get valuable diagnostic data from devices and instrumentation. Due to its inflexible nature, legacy fieldbus can also be harder to maintain and scale if the network infrastructure needs to change to support new technologies over time.

A modern industrial network protocol, such as EtherNet/IP, does not have these limitations. On EtherNet/IP, single-use equipment and instrumentation can be easily configured to communicate with and publish rich diagnostic data to the process control system. This communication builds into scalable plant-wide ethernet architectures through switches and other network devices. This plug-and-play connectivity creates a simpler plant infrastructure, with only power and ethernet cabling required to connect unit operations, and it allows for ease of expansion and easier equipment change-out.

Operational flexibility

Automation may not be on a producer’s mind when developing a new biologic or while in the early stages of clinical trials. It’s never too early to be thinking about automation because the optimal automation setup can provide significant operational flexibility and greatly reduce the effort involved in tech transfer.

Take the example of a start-up biologic company that invests in single-use equipment with a modern DCS. The equipment can be flexibly assembled into a process train and run manually during early process development, which allows settings to be changed as the process is being fully developed.

Once the company is ready to produce at a commercial scale, the equipment can be easily configured to run repeatable recipes with no major software updates, because the recipe is assembled from the same manual phases run in development. The equipment can even revert to manual operation if an issue arises where intervention is required.

Additionally, equipment can be repurposed and used in a different process because each individual piece of equipment has a full set of functionalities, essentially making each component a replaceable part.

PART 2: TECHNOLOGY AND SECURITY

Published February 9, 2022

Single Use Success in Life Sciences: Part 2
Single Use Success in Life Sciences: Part 2
Blog
Blog
Single Use Success in Life Sciences: Part 2
Life sciences companies establishing a single-use system with plug-and-play equipment need to set the right priorities early to ensure long-term success.
Topics: Accelerate Digital Transformation Life Sciences

John Hatzis
John Hatzis
Global Life Sciences Industry Consultant, Rockwell Automation
John has been with Rockwell Automation for eight years where he has gained expertise using Rockwell solutions in a variety of Life Sciences applications. In his role he also works with BiofabUSA and Biophorum. John has a degree in Chemical Engineering from Worcester Polytechnic Institute.
 
Pete Genest
Pete Genest
Former Strategic Technology Partnerships Leader, Cytiva
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs