Loading
Blog | Manufacturing Execution Systems
Recent ActivityRecent Activity

MES is Dead. Long Live MES.

Reports of the death of manufacturing execution systems (MES) have been greatly exaggerated.

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
MES is Dead. Long Live MES. hero image

2020 proved to be a critical time for the wide-scale rollout of industrial digital transformation initiatives. While this was already a trend throughout industrial organisations, the demand was fuelled, of course, by the COVID-19 pandemic, which presented a sudden and critical requirement for production agility and social distancing.

With more organisations implementing or scaling up digital technologies within their operations, manufacturers are continuing to look for ways to further optimise their Industry 4.0 investments. There are many ways to approach this, but one particularly impactful tactic is the removal of information silos between manufacturing systems. This includes Enterprise Resource Planning (ERP), Electronic Manufacturing Services (EMS), Manufacturing Execution Systems (MES), Manufacturing Operations Management (MOM), and other software systems and tools.

A holistic digital strategy helps manufacturers move faster by removing friction and data loss between disparate teams and systems. This “digital thread” is a communication framework that allows a connected data flow and integrated view of the asset’s data throughout its lifecycle across traditionally siloed functional perspectives.

By using a digital thread to connect data from all these sources, information can now flow between systems to inform and optimise business-driving processes for manufacturers.

Where Does MES Fit In?

The Manufacturing Execution System (MES) plays a key role in this. It records and validates every step in the process – from goods received to the finished and packed product. This is performed in conjunction with the other manufacturing applications, verifying that each production step has been completed as planned. Not only does this provide full traceability, it also delivers a rich set of data for further investigation and analytics to help producers create an information-driven manufacturing process that can help trigger actions or execute operations, activities, rules and more.

Many producers cannot compete on cost but instead need to implement systems that allow them to sell higher-quality, validated products. MES can verify and track material information, identify waste and overdosing, report inventory levels, and provide quality data, performance, and productivity for each order. Access to this kind of information opens avenues to better KPIs.

As such, MES plays a critical role in the overall approach. But what differentiates it from other solutions, such as ERP, Product Lifecycle Management (PLM) or the Industrial Internet of Things (IIoT)?

A Structured Approach

The key advantage of the MES is the structured way in which it stores the data based on events and transactions, while also verifying in real time that each step of the execution is performed correctly.

Consider this example: the ERP has an order that requires one of our nominal recipes to be extended based on the equipment capacity and capabilities. This means we need a new production recipe for the manufacturing floor, calculated from the nominal recipe generated in the PLM and the order in the ERP. The MES performs this logic and adjusts the required Bill of Process (BOP), Bill of Materials (BOM), and the related process parameters, then delivers these to the production floor.

Once the process is underway, the MES monitors every step, verifying and validating each activity and event, and storing the resulting data in a structured manner.

All this logic, and the necessary reaction time, is either not available or only partly available in a PLM, ERP or IIOT system.

An Information-Enabled Manufacturing Process

Working together, the MES, IIOT, ERP, PLM and other systems secure a common communication framework, allowing a connected data flow and an integrated view of the asset’s data throughout its lifecycle.

This single source of truth allows companies to focus on their business strategies, objectives and related KPIs, while the MES handles the “how?”, ensures that everything is working correctly, and calculates what’s need to fix errors when they do occur.

Not Extinct, but Evolving

MES is far from dead – it still has an important role to play in a digitally transformed operation. However, that role has changed, and MES is changing with it.

As the manufacturing process evolves, the MES is becoming more modular and flexible, incorporating the functionality needed to enable Industry 4.0. Together with IIOT, it provides increased interoperability, contextualised data, advanced analytics, and even the foundation for Extended Reality (XR) applications.

MES is evolving to become a more flexible part of an overall ecosystem of applications. And, in doing so, it is providing an essential part of the digital thread so critical to the success of Industry 4.0.

To find out more about the building blocks of any digital transformation, visit the Management Perspectives hub, where you’ll find a wealth of resources for executive industrial decision-makers.

Published March 24, 2021

Topics: MES Solutions Lifecycle Services Management Perspectives Aerospace Automotive & Tire Cement Chemical Entertainment Fiber & Textiles Food & Beverage Household & Personal Care Infrastructure Life Sciences Marine Mining, Metals & Cement Oil & Gas Power Generation Print & Publishing Pulp & Paper Semiconductor Water Wastewater

Uwe Küppers
Uwe Küppers
Manager, Consulting Services, Kalypso
Uwe Küppers has over 25 years' experience in the manufacturing industry. He has served in an advisory capacity on multiple projects for global companies, applying his expertise across analytics, IoT, and manufacturing enterprise software (MES). Uwe has been the EMEA Chairman of MESA since 2014.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs