Loading
Blog | Industrial Automation & Control
Recent ActivityRecent Activity

Scalability made easy with Logix Designer SDK

Bringing software engineering practices to automate workflows on your plant floor

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail

Pairing Logix Designer Software Development Kit (SDK) with Studio 5000 Logix Designer® allows users to automate many UI functions. Logix Designer SDK unlocks efficiency potential that was previously limited by manual workflows, resulting in reduced labor efforts, while improving speed of design, testing, and deployment. This includes supported file system operations, SD Card store and load capabilities, controller setting changes, and change tag values online and offline. Take a closer look at one use case that benefits from using the Logix Designer SDK.

ScenarioAn engineer is leading an improvement project to perform an area-wide controller upgrade in their facility. The area contains 30 cells, each with six different Logix controllers. The new install base will feature ControlLogix® 5580 processors at major revision 35. A copy of the upgraded project must be stored on all their SD cards. The controllers must also be set to Remote Run mode, in the proper order, to avoid interlock trips.

The Challenge

This migration is simple to perform on one controller, but at scale, could take quite a long time. Human error can be introduced by downloading the wrong project file, forgetting to load the project to the SD card, or enabling Remote Run mode in the incorrect sequence.

The Logix Designer SDK Solution

(Left, Manual)

(Right, Scripted)

Studio 5000 Logix Designer
male with glasses looking at a computer screen and typing on the keyboard
Studio 5000 Logix Designer

Studio 5000 Logix Designer® supports productivity while seamlessly configuring, programming, and maintaining the devices in your control system. 

Learn More

Figure 1

(Left, Manual): Time spent performing cell upgrade with traditional workflows. X represents misconfigurations resulting from human error.
(Right, Scripted): Time spent performing an upgrade using the Logix Designer SDK including an initial time investment for creating a script.

Figures 1 illustrates the time savings from the example scenario. With six controllers, the engineer saves 50 minutes leveraging the Logix Designer SDK (an estimated 20 minutes per upgrade per controller). The engineer also avoids having to correct for two errors in their work, for instance, downloading the wrong project file to the controller.

While six controllers can seem minor, the time savings are now multiplied for all 30 cells. The total labor would be 140 x 30, equaling 4200 minutes using the traditional Studio 5000 Logix Designer UI. The labor is now limited to the initial investment of 90 minutes for creating the script, as it can be executed the same on each cell.

Note: Results will vary depending on the complexity and scale of the operations to be performed.

The Result

By creating a script that iterates through a list of controllers and executes all required operations, the initial time investment can be longer, but afterward provide a significant time savings. Moreover, the Logix Designer SDK delivers consistency by limiting human error to the script's initial programming, rather than individual action instances. The real power of the Logix Designer SDK is scaling these benefits over dozens or hundreds of controllers, where the script can be reused. The return on investment for a small amount of up-front coding is evident immediately.

This use case demonstrates how the Logix Designer SDK brings a popular software engineering practice to industrial automation. Studio 5000 Logix Designer software configuration tasks are traditionally accomplished manually. The tools available in the Logix Designer SDK give the user possibilities and capabilities to transform manual, repetitive tasks into automated workflows, with the use of the software’s Application Programming Interface (API). As this use case showed, the time savings were immediate and vast. Logix Designer SDK functions such as example code, standard libraries, documentation, and debugging tools are available to help entry-level programmers take Studio 5000 Logix Designer functionality to the next level.

Published August 4, 2023

Topics: Integrated Architecture Software Studio 5000

Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe
Recommended for You
Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Com...
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs
  5. Chevron LeftChevron Left Scalability made easy with Logix Designer SDK