Loading
Blog
Recent ActivityRecent Activity

Improve Chemical Operator Effectiveness with a Modern DCS

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Improve Chemical Operator Effectiveness with a Modern DCS hero image

An information-enabled DCS helps workers turn data into actionable results.

Even with more information and greater automation, it’s still true today that successful chemical production depends on workers. But when you need to replace retiring seasoned staff with newer talent, how do you keep the same level of performance? Providing the right tools that empower workers to continually improve is a huge advantage of a data-enabled modern DCS.

A modern DCS is information enabled and connects all aspects of your chemical operations, including both automated and manual tasks. By giving operators clear, actionable information and avoiding non-essential data that can distract them, a modern DCS helps guide them through problems in real time.

This improves process visibility, decision-making and safety. As a result, you can have greater confidence that your new operators can soon become some of your best workers.

A Look Into a Modern DCS

A modern DCS uses a high-performance human machine interface, which provides critical information and guides operators to the right decisions during production and maintenance. This involves using a combination of proven situational-awareness techniques and graphic screen designs that enhance an operator’s focus and response time.

Chemical Producer’s Guide to DCS Migrations
Main Image
Chemical Producer’s Guide to DCS Migrations

Need to migrate to a new DCS and don’t know where to start? Watch Chemical Producer’s Guide to DCS Migrations Part 1: Planning.

Watch Webinar

Strengthen Your Workforce

These capabilities can benefit experienced workers just as much as they do new workers, especially if information is limited in your operation. In fact, when one chemical company replaced the control system across its plants with a modern DCS, it improved information gathering and financial reporting.

The company decided to implement the PlantPAx® DCS from Rockwell Automation. The new information-enabled system displayed real-time data, helping operators make better and more timely decisions. Additionally, the new system transformed data collection, data aggregation and reporting so insights could be shared on demand with business management for better decision-making and financial reporting.

As a result, the $16 million project paid for itself in just nine months, and the modern DCS will be used in four other projects within the company.

Reduce Downtime and Alarm Issues

Chemical operations are flooded with data from intelligent devices, which are designed to smooth operations and reduce downtime. However, this is only achievable if the raw data can be turned into actionable information.

A modern DCS can help. It turns diagnostic and performance data into actionable information that operators use to see if an equipment or production unit is nearing failure.

One chemical company needed to expand a unit to meet increasing market demand and chose to update its entire production unit to a modern DCS. The older control system was operating inefficiently, resulting in unplanned downtime.

The modern DCS delivers historical and real-time production data to plant operators in a clear, understandable format for easier analysis. Now, when an issue occurs, downtime is significantly reduced. Operators can easily pinpoint the issue using captured production and equipment performance data. As a result, the chemical company reduced ongoing downtime instances by 50%.

A modern DCS also helps reduce distracting, nuisance alarms and makes remaining alarms actionable. As a result, when alarms do occur, operators are guided by the DCS to immediately know what they need to do and how urgently they need to perform these actions. This helps cut troubleshooting time, costs and downtime.

The Choice is Yours

Whether you’re building a new chemical processing plant or replacing an existing control system, a modern DCS provides many benefits. It helps fill the knowledge gap for newer workers and offers actionable insights. It helps improve productivity and decision-making and helps make your overall business more successful.

Published July 8, 2020

Topics: Chemical

Chris King
Chris King
PlantPAx Migration Business Development Manager, Rockwell Automation
Chris has 40+ years of experience in Process Automation; with Rockwell Automation (3), Emerson (14) & Honeywell (23). Chris is responsible for developing Migration strategies, tools & methodologies to support Modernizations from legacy systems to PlantPAx. He is an SME with legacy DCS systems.
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs