Loading
Blog
Recent ActivityRecent Activity

Arena Simulation Software Can Improve Patient Care

Share This:

LinkedInLinkedIn
XX
FacebookFacebook
PrintPrint
EmailEmail
Arena Simulation Software Can Improve Patient Care hero image

Get it Right the First Time

This is a critical part in every industry, but even more so now in healthcare, when it quite literally means the difference between life and death.

What if you could answer “What if…?” questions before investing capital and without disrupting current operations?

What if:

  • …Our product mix, tact time, labor rules, failure rate, patient arrival rate, etc. changes?  How will that affect throughput, queues, costs, and resource utilization?
  • ….We add a shift, purchase a new machine, or change how we train employees? Will that give me the desired outcome?
  • …We consolidate two facilities into one facility? Do I improve efficiency or making everything twice as difficult?
  • …We build a new warehouse? Will the design present the best possible layout?
  • …I’m faced with a pandemic and our hospital is not designed for an inrush of critical patients?

Eliminate the Guesswork

Arena Simulation and advanced analytics predict the future and prescribe ways to optimize performance. Flexible, activity-based models can be used to simulate almost any process.

Quick (:57 sec) video model demonstrates activity in a typical emergency department and how adjustments can reduce waiting times for treatment.

Hospitals are using Arena to eliminate the guesswork and use factual data to help patients and save lives. While manufacturers use Arena – to efficiently change over operations and find the optimal way to stagger shifts, for example – hospitals model in Arena to anticipate the amount of resources they need for day to day operations.

We have supported field projects where there is uncertainty in the amount of resources needed, approaching scheduling problems to improve patient care, ambulatory routing, and more.

For example, we helped a cancer treatment clinic better manage patient care. A recent medical breakthrough meant more patients were surviving – and as a result, the number of appointments increased. Unfortunately, patient wait times exceed five hours.

The hospital needed to more efficiently stagger appointments to reduce those wait times and the long hours the medical staff was working. With simulation, the facility found the right combination of appointment/staff scheduling to ease the burden on both ends.

Keep Up With Changing Conditions

Pandemics increase the number of incoming patients and the number of specific resources needed. Adjusting the model to represent the anticipated patient increase allows hospitals to respond effectively.

COVID-19 has presented so much uncertainty, making us question what needs to be done and how fast we need to make changes. Factual data will help healthcare companies prepare to face whatever the next day might bring.

Resources in New York, like other large metropolitan areas, are stretched thin. As the anticipated number of patients increases, hospitals must respond quickly to provide as much care as possible. Here’s just one example of simulation software in action: Northwell University and Lenox Hill Hospital teamed up to convert their pediatric outpatient surgery area into an adult intensive care unit and used Arena to become as efficient as possible – and save lives.

Data helps decision-makers understand the flow of systems and the constraints of resources, including doctors, nurses and equipment. Planners can prepare for pandemics, flu season, natural disasters, and caregivers can be ready.

Published May 20, 2020

Check Out These Related Case Studies

  • Cancer Treatment Facility Reduces Patient Time in Clinic by 25 Percent with Arena Simulation Software
  • Arena on Healthcare Crisis Operations
  • Arena: Doing More with Less

Tyler D. DiFrischia
Tyler D. DiFrischia
Arena Simulation Account Manager, Rockwell Automation Inc
Connect:
EmailEmail
Subscribe

Subscribe to Rockwell Automation and receive the latest news, thought leadership and information directly to your inbox.

Subscribe

Recommended For You

Loading
  1. Chevron LeftChevron Left Puerto Rico
  2. Chevron LeftChevron Left Company
  3. Chevron LeftChevron Left News
  4. Chevron LeftChevron Left Blogs