Control Station, Inc.
PlantESP Loop Performance Monitoring leverages existing process data to identify issues stemming from underperforming PID controllers. With the Summer 2021 release users benefit from the introduction of advanced state-based analytics and the ability to apply multifaceted logic for the purpose of defining a full spectrum of process conditions. Specifically, users can:
- Easily define a PID control loop’s many different conditions using PlantESP’s intuitive logic configurator. Gain insight into loop performance as a given PID regulates control throughout various phases of production.
- Generate custom reports that reveal the true nature of a facility’s critical processes. Expand or collapse the different categories of state-based intelligence for effective analysis and decision-making.
- Capitalize on a streamlined user interface and put the latest PlantESP improvements to work with a single click. Reduce the work associated with configuring reports and other common administrative tasks.
PlantESP has been successfully deployed across the process industries.
Available for sale: Available now

For more information, contact:
View all the new products and solutions
Automation Fair features the newest innovations from Rockwell Automation and members of the PartnerNetwork™.
Learn more about these technologies by visiting the exhibit hall at the event. Automation experts will be ready to discuss how you can advance your operation.